4/3/2008 2:35 PM | |
Joined: 4/26/2007 Last visit: 1/19/2024 Posts: 120 Rating: (8) |
Hi, I use PLCsim with Step7 but never with WinCC flex. I think it is not possible. Or yes??? PLCsim -> Step7 WinCC flexible rutime simulator -> WinCC flexible IntroductionS7-PLCSIM enables you to run and test your STEP7 user program on a simulated programmable logic controller (PLC). The simulation executes on your computer or programming device, such as a PG 740, Power PG or Field PG. Because the simulation exists completely within the STEP7 software, you do not need to be connected to any S7 hardware (CPU or I/O modules). You can use S7-PLCSIM to simulate STEP7 user programs that were developed for S7-300, S7-400, and WinAC controllers. S7-PLCSIM provides a simple interface to the STEP7 user program for monitoring and modifying different objects such as input and output variables. You can also use the various applications of the STEP7 software while you are running your program on the simulated PLC. This allows you to use such tools as the variable table (VAT) to monitor and modify variables. S7-PLCSIM Features You can use S7-PLCSIM to perform the following tasks:
|
Last edited by: potretma at: 4/3/2008 2:39 PMLast edited by: potretma at: 4/3/2008 2:35 PMLast edited by: potretma at: 4/3/2008 2:35 PM |
|
4/3/2008 3:43 PM | |
Posts: 3 Rating: (0) |
I'm sorry, but PLCSim + WinCCFlexible Runtime work very good. For example S7-314 + MP277 |
Follow us on