1/8/2013 10:41 PM | |
Joined: 9/27/2006 Last visit: 5/14/2024 Posts: 12257 Rating: (2668)
|
Hello edsan; Integration of the WinCC Flexible in Step 7 does not require any external package (such as Sm@rt Client). See this FAQ: How do you integrate a WinCC flexible project in STEP 7? You should start by completely installing your Step 7 with all additional packages required for your application(including the F-System, the Safety matrix and the CFC programming language, see the following link: https://www.automation.siemens.com/mcms/simatic-controller-software/en/programming-options/s7-f-fh-systems/s7-f-systems/pages/default.aspx?HTTPS=REDIR); Hope this helps, Danoiel Chartier Note: if you are curious about the Sm@rt services (Sm@rt servers and Sm@rt clients), here are links to a manual and a list of FAQs on the subject: SIMATIC HMI WinCC flexible 2005 Sm@rtAccess, Sm@rtService: "Sm@rtAccess and Sm@rtService are the options available in WinCC flexible for communicating between HMI systems or to an HMI system by means of TCP/IP connections (for example, LAN)." WinCC flexible Options -- Product information -- WinCC flexible /Sm@rtService (Teleservicing) |
Last edited by: dchartier at: 1/8/2013 10:46 PM |
|
1/9/2013 9:08 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello, you have to install STEP 7 V5.5 first and second the WinCC flexible. Consider the correct software version of WinCC flexible in refer to Windows. See also the informations of the FAQ: http://support.automation.siemens.com/WW/view/de/18734363 With best regards |
9/18/2013 9:32 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
New question was splitted to integration to my win cc. Best regards O_Moderator |
Follow us on