6/19/2012 4:26 PM | |
Posts: 3037 Rating: (192)
|
Hello weighting, Perhaps you can use ProAgent for this. You can see an example of ProAgent with WinCC flexible in the following link. Process diagnostics with SIMATIC S7-PDIAG and ProAgent based on LAD/FBD/STL and S7-GRAPH Tweety |
6/20/2012 3:12 PM | |
Posts: 3037 Rating: (192)
|
Hello weighting, |
6/21/2012 2:27 PM | |
Posts: 3037 Rating: (192)
|
Hello, I have checked this project with Step 7 V5.4 + SP4 and WinCC flexible 2008 SP2 Update 13. I can open the project of Step 7 and the project of WinCC flexible too without errors. With which software do you get this fault? you shouldstorethis project local on your computer not on a network drive.. You can find the error in the following FAQ: Which meaning have the error codes (xxxx:yyyy) in STEP 7? Tweety |
6/22/2012 1:51 AM | |
Posts: 17 Rating: (0) |
Hello Tweety! I stored this projectunder D:\Program Files\Siemens\Step7\S7Proj,do this store method not correctly? |
6/22/2012 2:12 PM | |
Posts: 3037 Rating: (192)
|
Hello, This path seems ok. You should test shorter path for this project, for example "d:\test". Tweety |
Follow us on