4/18/2016 8:16 AM | |
Joined: 3/14/2008 Last visit: 7/20/2024 Posts: 2078 Rating: (931) |
Hello, What license popup do you get? There can be multiple issues: Wrong version license, more than one license of the same package, corrupt license, etc. In the bottom right of the screen (icons on the taskbar), you can right click on the WinCC icon called: Simatic WinCC RT and then select: "WinCC license analysis". Please report back the screen you will get. Maybe you can even see what license is missing or not correct. |
If I could help you, you can use the RATE button. Thank you. |
|
4/18/2016 2:14 PM | |
Joined: 3/14/2008 Last visit: 7/20/2024 Posts: 2078 Rating: (931) |
Is your project created with PCS7 or normal step7+WinCC. What version are you using btw? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on