10/11/2020 8:10 PM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942)
|
Hi, The easiest answer: snapshots are not supported. It looks like the main server has detected an outage of the redundant server because of the snapshot. This most likely issued a reboot. So solution: Do not take snapshots of if you really want only without WinCC runtime but as said: snapshots are not supported. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on