10/25/2022 8:53 AM | |
Joined: 2/17/2020 Last visit: 6/10/2024 Posts: 1009 Rating: (178) |
Hi luka31, Formally full functionality of the Audit Trail is not available in WinCC Professional, although you can use, among other things, alarming to implement these tasks. This is described at the following link: GMP Engineering Manual SIMATIC WinCC (TIA Portal) V15 - Configuration for WinCC RT Professional Hope that helps. |
A rating will be well appreciated. |
|
This contribution was helpful to1 thankful Users |
10/31/2022 10:21 PM | |
Joined: 4/3/2017 Last visit: 5/15/2024 Posts: 69 Rating: (1) |
Is it possible to save user actions from buttons from faceplates? |
11/3/2022 3:00 PM | |
Joined: 2/17/2020 Last visit: 6/10/2024 Posts: 1009 Rating: (178) |
Hi again, Yes, it should be. Please refer to the following section of the manual: Creating operator input alarms - Operator input alarms in combination with faceplate types |
A rating will be well appreciated. |
|
Follow us on