3/15/2023 3:22 PM | |
Joined: 5/6/2022 Last visit: 5/16/2024 Posts: 420 Rating: (83) |
Hi GBarthelemy, I will try to explain as clearly as possible. From what I understand, you have already integrated the servers in STEP7 classic (being redundant servers, to make the load to these, it is done from STEP 7) and now what you want is to add those two clients without their own project. That said, what I recommend you, is that the most normal thing would be to integrate everything from SIMATIC Manager, but you can also not do it and simply configure them in wincc explorer and do the interconnect in simatic shell. For the method that I am telling you, since you have the servers in step 7, you can include them there also following what it says in the manual that I put below: "SIMATIC HMI WinCC V7.5 WinCC Information System: Integration of WinCC in SIMATIC Manager" I hope I have been able to help you or at least guide you with your doubts. Best regards! |
If this Information really helps, you could use the Rate function |
|
3/16/2023 9:55 AM | |
Joined: 8/3/2009 Last visit: 5/17/2024 Posts: 12970 Rating: (1651)
|
Hello GBarthelemy Clients without projects you do not have to integrate in SImatic Manager. you have to add them only in the computernamelist in WinCC project Check this FAQ: https://support.industry.siemens.com/cs/de/en/view/109771695 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on