3/10/2014 8:38 AM | |
Posts: 1299 Rating: (136)
|
Hello, you can add the unit in properties of the IO field, "Appearance> Unit" K!ke |
This contribution was helpful to1 thankful Users |
3/10/2014 3:16 PM | |
Posts: 1299 Rating: (136)
|
Hello, you can just type in the field the symbol + C. I tested it and there was no problem. K!ke |
3/11/2014 7:45 AM | |
Posts: 1299 Rating: (136)
|
Hello, |
4/22/2014 10:54 AM | |
Posts: 340 Rating: (6) |
new question is splittet to How can I display external tags Date, Time_Of_Date, Date_And_Time |
6/24/2014 1:57 PM | |
Joined: 11/4/2011 Last visit: 8/25/2024 Posts: 253 Rating: (53) |
Hi. There is such document, located in Windows. It is called Character Map. See how to open and use it at symbolcodes.tlt.psu.edu and microsoft. You can also press Win+R and type charmap. OK. A Degree sign is not a Unicode character, it is ASCII and has a number of 248 in the ASCII Character Map. So you can do this way: hold Alt and type one by one: 2 4 8 (on the NUM PAD!), then release Alt. Pay attention when using the Unicode symbols such as ² ³ ← ↑ → ↓. They could not be displayed with Tahoma Font. Use Arial instead. |
Follow us on