10/24/2014 10:49 AM | |
Joined: 2/6/2009 Last visit: 6/10/2024 Posts: 46 Rating:
|
Hello, How can I configure WinCC TIA V13 Professional to plays sound on incoming alarm, same as HORN functionality on standard WinCC V7.3 (or earlier)? Is this supported by WinCC V13 Professional? WinCC V13 Professional manual say's some thing about annunciator, but is not clearly explained how to configure it, or if it can be used to play sound file (.wave for example) or it only purpose is for external (real) horn or sound alarm indicator (light+sound column etc.). I have expirience in standard WinCC 6.2 till 7.3, but now i have new project in WinCC TIA V13 Professional, and it is hard to adopt to new interface and features. I know that I can use script mentioned onlinkand apply it to every alarm as triger, but can it be done by sistem functionality like in regular WinCC Horn editor? BTW on uper link you have to change the name of header from "apdefap.h" to "ap_def.h", in order script to work under WinCC TIA V13 Best regards, Vlad |
Last edited by: VladD at: 10/24/2014 3:42 PMLast edited by: VladD at: 10/24/2014 3:37 PM |
|
10/28/2014 7:20 AM | |
Posts: 1299 Rating:
|
Hello, in WinCC Runtime Professional it's called "Alarm annunciator" https://www.automation.siemens.com/mdm/default.aspx?DocVersionId=63974837515&Language=en-US&TopicId=59058819723 K!ke |
7/24/2017 12:04 PM | |
Posts: 1 Rating:
|
I could not see that document file. |
7/27/2017 4:14 PM | |
Joined: 8/25/2005 Last visit: 7/5/2024 Posts: 1161 Rating:
|
Hello Special Kyaw, I'm able to open the link Please check the document WinCC Professional V13.0 SP2 and search there for Alarm annunciator. Hope this will be helpful. Good luck |
This contribution was helpful to
1 thankful Users |
Follow us on