4/18/2021 11:53 PM | |
Joined: 1/15/2018 Last visit: 10/20/2024 Posts: 18 Rating: (0) |
Good morning all, I have a random issue in where some functions (toggle button screen run by C scripts) sometimes lock up / lag for 30-60 seconds. Whilst this is happening all dynamic points are still updating and I am able to navigate elsewhere in the runtime without issues. The script is common to all of the buttons which are causing issues. I would like to be able to understand the diagnostic functions of WinCC but am a bit overwhelmed with all of the documentation. Here is the script below. Thanks [snip]
Attachmentscript.txt (108 Downloads) |
Last edited by: Jen_Moderator at: 04/19/2021 11:17:09Added script as a txt file. |
|
Follow us on