2/18/2021 9:33 PM | |
Joined: 12/13/2011 Last visit: 4/19/2023 Posts: 123 Rating: (14) |
It seems there was something wrong with my install :(. I will update once I have figured out the issue. |
4/19/2022 11:45 AM | |
Joined: 11/8/2019 Last visit: 12/23/2022 Posts: 1 Rating: (0) |
Do you know what went wrong? I have the same issue. |
9/26/2023 11:36 AM | |
Joined: 1/21/2013 Last visit: 9/25/2024 Posts: 3130 Rating: (489)
|
Hi Jarb77, Do you have the WinCC Unified PC RT software installed? For WinCC Unified V18 this is no longer bundled with the TIA Portal software and must be installed separately. Kind regards |
9/26/2023 1:40 PM | |
Joined: 1/21/2013 Last visit: 9/25/2024 Posts: 3130 Rating: (489)
|
Hi Jarb77, Yes, your screenshot shows that you have WinCC Unified PC RT software installed. However, since you have installed V18 Update 2 for the engineering software, I would recommend that you also install an update for WinCC Unified PC RT. When creating a configuration on your system, device version V18.0.0.2 is selected by default and to be honest, I am not sure if simulation will work with an older version of PC RT. You should also run the "WinCC Unified Configuration" to adapt your settings to your computer. You would have been asked to do this during the installation, but you are not forced to do it. If the PC RT is installed, your browser should display the WinCC Unified page when you access https://localhost or https://127.0.0.1. Note: Your browser may block the connection in this case because the certificate is created for your computer. Therefore, you must enter your computer name instead of localhost. When you view the details of the browser message, you should see the expected computer name. Kind regards |
Follow us on