8/23/2022 11:22 AM | |
Joined: 2/12/2019 Last visit: 4/3/2024 Posts: 10 Rating: (1) |
Hi people, is there away to change the background of IO field to transparent? i have 2 IO fields displaying date set to output mode but i do not have the option to set transparency, i can only change the background colour to match the rest of the display however it sticks out and is quite evident. now i can display this as a text box but then i am stuck with hh.mm.ss and i am unsure how to trim in unified. i could convert it to a string and do it through the PLC but i feel like there should be an easier way of doing this. any help would be grateful. Thanks AttachmentDate_unified.zip (196 Downloads) |
Follow us on