10/8/2020 11:16 AM | |
Posts: 30 Rating: (1) |
Hi experts, We are using IPC547E running WinCC v7.5 Sp1 Upd4 as Server and 1 Simatic PG as OS client. The WinCC runtime after running about 1-2 days, operator has complaints not able to perform change page, button click action on the OS Server, but OS client has no issue. We try to exit the runtime of OS server and start back the runtime, but it was not successful and pop up error 'No connection to the script control. We are not able to open any C-script also in wincc explorer. Thus, we suspect is the script.exe is not running somehow. Then we execute the script.exe, everything back to normal. We have extracted the wincc diagnose file, refer attachment 'Diagnose.zip'. We are not sure what was happening. Attachmentdiagnose.zip (99 Downloads) |
Follow us on