1/26/2024 9:18 AM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641)
|
Alex.P means if you work in Windows with the user with you have installed WinCC? Because there are made several special user groups with installation and the install-user is set to it. If you would use another user then you would have to set it into the usergoups manually. Do you have installed the latest Update: https://support.industry.siemens.com/cs/de/en/view/109818723 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on