6/13/2011 9:53 AM | |
Joined: 3/31/2009 Last visit: 1/22/2024 Posts: 191 Rating: (3) |
Hii, how can i fire/execute second button onclick event from first button using vbs. br rusli
|
6/13/2011 10:05 AM | |
Posts: 487 Rating: (36) |
Hi Why not re-use the code behind the second button together with the code in th first button. Eric |
6/13/2011 10:12 AM | |
Joined: 3/31/2009 Last visit: 1/22/2024 Posts: 191 Rating: (3) |
cannot do that, the first button use vbs the second button use c |
6/13/2011 8:38 PM | |
Joined: 10/3/2010 Last visit: 5/17/2024 Posts: 1552 Rating: (188) |
depending on what you want to achieve, maybe it's possible to fire the second script via a global action script instead of mouse left release, where an internal tag set in the first script is used as condition to start the global action? |
B r g d s , |
|
This contribution was helpful to1 thankful Users |