6/27/2023 7:41 AM | |
Joined: 12/7/2020 Last visit: 5/23/2024 Posts: 31 Rating: (1) |
TIA Portal V16 update 5 WinCC Professional V16, SIMATIC Logon Hello! Few days ago I create an Operator Event logging scripts connected to a faceplate an get a lot of warnings (about 900):
Thing is i link an Release button event outside (Pic 1 and 2), and create C script with TriggerOperatorEvent method. So... in Client Runtime everything is working all right, but when i start WebNavigator on other machine i get ~10 Errors (for every screen that faceplate is used - picture 3) After suppressing all errors, everything is working correctly. Attachmentforum.pdf (261 Downloads) |
Last edited by: Scyzoryk96 at: 06/27/2023 07:42:44attachment change Last edited by: Scyzoryk96 at: 06/27/2023 07:43:37syntax correction |
|
6/27/2023 10:09 AM | |
Joined: 5/6/2022 Last visit: 5/23/2024 Posts: 420 Rating: (83) |
Hi Scyzoryk96, Some time ago I remember seeing an error related to the 'TriggerOperatorEventError' function and I remember that it was solved with the version of TIA Portal V17 update 6. But I understand that it is still not the solution since you have a lower version. That's all I can tell you. Best regards!
|
If this Information really helps, you could use the Rate function |
|
6/27/2023 3:15 PM | |
Joined: 12/7/2020 Last visit: 5/23/2024 Posts: 31 Rating: (1) |
Unfortunately, it didn't help. It make it worse somehow because Logging in WebNavigator stopped working |
Follow us on