Industry Online Support
Technical Forum
2/2/2010 9:09 AM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hi Sumair, I'm not related with a tutorial or something but you could have 3 approaches. 1. Setup an ad-hoc network if possible with the WLAN cards in your PC. This is a solution to connect 2 WLAN Clients with each other. This is not a very secure way to do this since it's an old technology and it's officialy only support for IEEE 802.11b networks (max. gross bandwidth is 11 Mbps). 2. Use an Access Point to connect both PC's with. Very easy but you need to setup 3 components. You can use the most secure technologies and you can use IEEE 802.1 a/b/g/h which will give you more speed (up to 54 Mbps) and you can use the 5 GHz frequency if allowed in the country where this application is located. 3. Connect one PC to an Access Point and connect the other PC with a WLAN card. Same benefits as number 2. |
Best regards, |
|
Follow us on