4/15/2011 9:30 AM | |
Posts: 21 Rating: (1) |
heloo
Splitted from Distributed safety. AttachmentDiagnose1.zip (192 Downloads) |
Last edited by: O_Moderator at: 4/15/2011 11:02 AMnew subject after splitting |
|
4/16/2011 7:56 AM | |
Posts: 21 Rating: (1) |
Dear thanks for replay i attached the program
i need some help about cpu315F , icommission a new CPU 315F it is in Running mode i did some signal Test during work i found one of the Analog card have wrongconfigurationtype i made it correctand download theoriginalprogram with this HWConfig rationChanging, but this time CPUgo in stop mode ididn'tknow the password but i give 3618 this we are using mostly in our systems. Please help Best Regard Bukhari AttachmentHot_Gas_.zip (193 Downloads) |
4/16/2011 3:28 PM | |
Joined: 10/7/2005 Last visit: 4/28/2024 Posts: 3004 Rating: (1046)
|
Hello Bukhari not too sure how you managed to end up in this situation, but I'm afraid to say that it doesn't look good. Based on your description, Diag buffer and S7 project,you have at least the following problems to sort out first: 1.) The HWconfig of your (online backup?)S7 project does NOT have any Safety I/O cards in it. It doesthough show "Standard Modules" without part number nor type instead of what presumably are meant to be Safety I/Omodules. This HWconfig is NOT going to work. 2.) The CPU does NOT have the tick for "CPU contains Safety program" in the "Protection" tab of its properties! This is NOT going to work if you have a Safety related application and Safety I/Omodules. The only way forward that I can see to fix this is that you firstly get hold of a useable offline backup of the S7 project. I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on