6/20/2016 9:57 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello tekabi; Why would you want to limit interventions from forum members to "experts"? Don't you think that replies from enthusiastic amateurs can sometimes be a lot more informative and helpful when you face a problem? To answer your question simply: no. Unless you have some kind of analog-to-digital circuit that can decode the 16-bit analog value to 16 digital signals; then you could connect these to 16 digital inputs, read them all together as a single word, convert the reconstructed analog value to an engineering value... Sounds like a lot of time, design and trouble that could be easily avoided by locating and EM231 module and using scaling functions of Microwin. Hope this helps, Daniel Chartier Edit; If you do want to study the requirements for Freeport comms on the S7-1200, you could look at the following Discussion; our friend JBell proposes a link to the S7-200 Tips and Tricks that proposes a few sample programs using Freeport communications. https://support.industry.siemens.com/tf/ww/en/posts/6183/ But you will need some kind of analog-to-serial converter, either as a single-chip microcontroller, or an Ardyuino/Rasberry PI project, in order ot generate the converted analog value and transmit it in a form that can be understood by the Freeport protocol. D.C. |
Last edited by: dchartier at: 6/20/2016 10:25:29 PM |
|
This contribution was helpful to4 thankful Users |
6/21/2016 4:59 PM | |
Posts: 5225 Rating: (1185)
|
(1) Else (amateur answer) build/buy a circuit to convert
(4) w |
This contribution was helpful to1 thankful Users |
Follow us on