2/14/2020 9:30 AM | |
Posts: 1 Rating: (0) |
Hi All, Is there a way to check how much room I have in the controller for new blocks? Or is there any data about limits for each type of a controller (i.e. PXC100)? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/14/2020 09:57:54New subject after splitting Last edited by: Fru at: 02/14/2020 10:24:28 |
|
2/14/2020 3:52 PM | |
Joined: 6/4/2010 Last visit: 4/27/2024 Posts: 374 Rating: (126)
|
Dear forum member, Please navigate from CFC to «Option» => «Customize» => “Compile and Download”. You can find the number of used DBs in the open window then. Please see attached print screens for further information. Please make sure you stay within the maximum limit according to the Desigo PX system documentation “Desigo™ Building automation system 6.2 Update, Technical Principles”, CM110664en_06. Best practice is to stay 10% below the maximum value to have room to add addional objects in case of application program changes and to avoid a high cycle time. Best regards, Albis AttachmentMenu_DB-Count.docx (451 Downloads) |
2/29/2020 1:59 PM | |
Joined: 4/5/2013 Last visit: 4/11/2024 Posts: 3 Rating: (1) |
The following info (link) is also worth considering, if necessary: https://support.industry.siemens.com/cs/document/109774921/desigo-pxc-(e)-d-trend-align-(algnivl)-feature-behavior-in-case-of-big-application-programs?dti=0&pnid=24186&lc=en-FI |
Follow us on