Industry Online Support
Technical Forum
6/27/2011 4:21 PM | |
Joined: 12/1/2006 Last visit: 6/27/2024 Posts: 26 Rating: (0) |
Siemens ...\ STEP 7 \ EXAMPLES \ zEn18_01 Where can I find |
6/27/2011 6:24 PM | |
Joined: 9/27/2006 Last visit: 7/1/2024 Posts: 12266 Rating: (2674)
|
Hello Huseyin; From the FM451 Positioning Module v. 5.x manual: http://support.automation.siemens.com/WW/view/en/1118070 12.1 Introduction When you install the FM 351/FM 451 configuration package, a sample project is also installed that illustrates several typical applications based on a number of selected functions. The English sample project is in the following folder:...\STEP7\EXAMPLES\zEn18_01 This contains several S7 programs of varying complexity and with different aims. So, if you have installed the configuration pack, the zEN18_01 sample program should already be installed on your computer, wherever you have selected the Siemens directory to be located when you first installed Step 7. If you cannot locate it, simply do a Search for the Siemens directory on your harddrives. If you do not have it yet, the FM 351/FM 451configuration package can be downloaded here, check it out: http://support.automation.siemens.com/WW/view/en/29851303 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on