4/1/2014 2:37 PM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of the User NBahri
|
4/1/2014 8:41 PM | |
Joined: 9/27/2006 Last visit: 9/10/2024 Posts: 12282 Rating: (2683) |
Hello NBahri; If you read the S5 to S7 conversion manual, you will see that LIR/TIR instructions (Load indirtect register/Transfer indirect register) cannot be translated to S7 programs. You must start by decoding what the S5 programmer was trying to do with these instructionsand reprogramming these sections in Step 7. Start with the following thread: LIR and TIR commands translation Then look at this collection oif discussions on the same issue: Hope this helps, Daniel Chartier |
4/2/2014 12:33 AM | |
Posts: 1 Rating: (0) |
pleas can y help how to correct one error then iwill try to change the other pleas help me |
Follow us on