Industry Online Support
Technical Forum
6/2/2014 8:27 AM | |
Posts: 8946 Rating: (999) |
That IP262 is a closed Loop controler. Parameter are stored as DB inside the CPU. But you have take care of the small Switches / Dip Switches! |
6/2/2014 2:56 PM | |
Posts: 29 Rating: (0) |
Thanks for your reply, So i don't have to program it. But why there is a PG port in the card?
|
6/2/2014 4:48 PM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308) |
Hello isteak You can download the manual of IP262 from here : Closed-Loop Control Module IP262 I have never used this module, but as per the manual ( Section 2.1 ) , the IP262 is a self contained Intelligent unit which can be used as Stand alone, ina CPURack or on SINEC-L1. You can study the manual in detail, but from what I have understood... the Controller structures are stored on the Module and parameters can be adjusted from a CPU / Over SINEC-L1 or using a HMI / PG. So obviously you cannot just replace the module. You will have to transfer the Module controller structure to the new module before replacement. Hope this helps Cheers Navnag |
Last edited by: Navnag at: 6/2/2014 4:48 PMThere is no such thing as the last bug in a program |
|
Follow us on