11/5/2008 3:42 PM | |
Joined: 11/21/2007 Last visit: 6/20/2024 Posts: 2324 Rating: (307) |
Hi I am using a S7-300 with 6RA70 drives V2.2 and V3.1 connected over Profibus using CBP2. When I access the drives from within Simatic Managar, I can Go Online and view all drive parameters, however I connot modify any parameter except P051. When I try I get a msg : "No Control Command acceptance". ( Screenshot is attached ) The drive is otherwise working and communicating fine on Profibus. Also if I connect to the drive using DriveMonitor and Serial port of the same PC, I am able to access anc modify all parameters. Can anyone shed some light on the problem ? Thanks Navnag AttachmentDrives_ES_Screenshot.zip (239 Downloads) |
There is no such thing as the last bug in a program |
|
Follow us on