Industry Online Support
Technical Forum
8/23/2012 3:24 PM | |
Posts: 767 Rating: (69) |
Hello hotan_levent, Copy and paste from original question: I have power cable for servo motor which code 6fx5002-5cn01-.... so there is N in code, what is that? I have never seen this code and I have used 6fx5002-5ca01-.... for power connect. The cable has 500 and normal connect characters so the new cable with N code has connect 500 and speed connect characters. what is the difference?
Feedback: These power cables such as6fx5002-5cn01-.... so there is N in code are equiped with a different type of connector for motor. The power cables with the "a" after the "c" in part number above have a fully threaded connector which requires rotating the cables several turns for complete connection to motor. The power cables with the "n" after the "c" have three catch studs to where with only 1/4 turn clockwise rotation the connector is locked. Likewise only 1/4 turn counter clockwise rotation the connector is unlocked. These cables can only be used used withthe following motors from Siemens: 1FT7... 1FK7 Generation 2 Motors (i.e. redesign) Consists of motors that have part number beginning with 1FK7xxx-2xxxx-xxxx, 1FK7xxx-3xxxx-xxxx,and 1FK7xxx-4xxxx-xxxx. 1PH808x and 1PH810x motors with power connector to use SPEED CONNECT cables. Unfortunately, I can not provide feedback on price since this could depend upon your local sales team. Attached is a pdf showing the major difference and a brief pictoral of which motors can use SPEED CONNECT cables. Following is main features description of benefit forthe SPEED CONNECT cables: §Installation and service expenditure reduced due to quick-release lock §Fail-safe installation through defined locked position §Approx. ¼ cw rotation and the connector is locked ! §Approx. ¼ ccw rotation and the connector is unlocked ! Deputy AttachmentC:\Documents and Settings\summrl\My Documents\FY12\Reference\Forum\SPEED CONNECT\SPEED CONNECT.pdf (594 Downloads) |
8/24/2012 10:36 AM | |
Posts: 59 Rating: (2) |
HiDeputy Your Message is clear everything and the message was too injured. thanks my friend.
|
Follow us on