7/7/2011 3:55 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Hello, For sure using a virtual machine will solve the problem with compatibility. Take a look at http://www.microsoft.com/windows/virtual-pc/default.aspxor in case your processor doesn't support virtualisation look at www.vmware.com Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
7/10/2011 1:50 PM | |
Posts: 5 Rating: (0) |
Virtual machines are very usefull in this case, and also there are some other solutions. for example Digsi 4.83 can not be installed on windows 7 , but you can download an update file from http://siemens.siprotec.de/download_neu/index_e.htmto upgrade Digsi 4.83 to Digsi 4.84, that is compatible with windows 7. Maybe you can find more solutions for next software in this website. be successful |
This contribution was helpful to1 thankful Users |
2/23/2012 12:34 PM | |
Posts: 1 Rating: (0) |
Hello Sir I am useing Windows 7 ultimate 32 Bit and i am able to use all the software of simens .. I suggest use Windows 7 ultimate 32 bit if you facing any problem with your software.Simens software compatibility with windows 7 ultimate is awesome . |
3/4/2012 2:34 PM | |
Posts: 197 Rating: (3) |
Hello adamstuart07, Just curious to know how much RAM have you installed on your PC/Laptop and how much does the OS reports? Also, which version of Step7, WinCC Flex,etc? Regards |
5/21/2012 5:53 PM | |
Posts: 197 Rating: (3) |
@ adamstuart07: "Simens software compatibility with windows 7 ultimate is awesome ." Absolutely. Simatic Manager sits on Win 7 32-bit very "peacefully" and without "any complaints" during installation / setup. Like they are made for each other. Also, WinCC Flex 2008 was very co-operative. They are absolutely compatible with Win 7. My configuration: Fujitsu Lifebook i5-430M 4GB RAM 320GB HDD Win7 Ultimate 32-bit SP1 , Step7 V5.5 sp1, WinCC Flex 2008 SP3. Regards |
5/21/2012 10:14 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (153) |
I am using XP Modeunder Win7 64- bit. |
Follow us on