1/23/2024 7:34 PM | |
Joined: 6/11/2019 Last visit: 10/18/2024 Posts: 2287 Rating: (99) |
Hello, Use VM storage.Maybe this will help you. Greetings Ella_68 (translated with Google) AttachmentProgrammplan-1.zip (314 Downloads) |
1/23/2024 8:10 PM | |
Joined: 6/11/2019 Last visit: 10/18/2024 Posts: 2287 Rating: (99) |
Hello TwistedTeknician, How about this?? Good night, Ella_68 AttachmentProgrammplan-2.zip (304 Downloads) |
1/24/2024 9:51 PM | |
Joined: 6/11/2019 Last visit: 10/18/2024 Posts: 2287 Rating: (99) |
Hello TwistedTeknician, Once again you can see that the simulation does not always reflect the true logo. The problem was a time problem in processing. I replaced the AND with the positive edge (B007) with NAND with the negative edge. By using the signal length TH of B005, I give B002 additional time to adopt the values from NAI1. Greetings Ella_68 (translated with Google) AttachmentProgrammplan-2a.zip (328 Downloads) |
Last edited by: Ella_68 at: 01/24/2024 22:06:40typo corrected |
|
1/25/2024 1:49 PM | |
Joined: 7/1/2023 Last visit: 5/15/2024 Posts: 67 Rating: (0) |
Good Morning Your new program works perfectly so I am glad the AM2 module has not failed. I have now modified them a bit but have run into an issue. I am trying to have Auto Random behavior or Manual control via LWE webpage. If you look at the attached files, you will see that Auto Random works fine but manual control does not. The slider keep snapping back to zero and I don't see what is going on. I think an analog input is required and associated to the AQ in manual mode but I can seem to get it. Your thoughts please? And, as always, your time and help is very much appreciated AttachmentVariable or Manual Control.zip (314 Downloads) |
1/25/2024 9:38 PM | |
Joined: 6/11/2019 Last visit: 10/18/2024 Posts: 2287 Rating: (99) |
Hello TwistedTeknician, You're making a typical beginner's mistake . You cannot define an output or flag twice. By defining the output AQ1 in the LWE, it is no longer available for the logo program.You have to integrate the values from the slider into the program via a free marker or analog network input and switch between manual and random using a muxer. The OR connection doesn't work like that either. If either switch is on, the function of the other is blocked. It is then easier to switch over using a button and to use a pulse relay. The status of this relay can then be displayed in the LWE via a network output or marker. I added these changes to my original example. I hope I can help you with this. Greetings Ella_68 (translated with Google) AttachmentProgrammplan-2a-LWE.zip (318 Downloads) |
Follow us on