2/11/2018 7:14 AM | |
Posts: 4 Rating: (1) |
Dear all before i was using windows xp with drivemon already installed and working, but windows 10 not able. how make it with windows 10 |
2/11/2018 7:22 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Hello, Which drivemonitor version do you have.? Windows 10 is 32 or 64 bit? You need to have drivemonitor V5.5 SP2, windows 10 64 bit. Please check below FAQ. DriveMonitor Version V5.5 SP2 for SIMOVERT MASTERDRIVES, MICROMASTER and SIMOREG. |
Last edited by: Jen_Moderator at: 2/12/2018 12:05:44 PMOptimized link. |
|
2/11/2018 7:57 AM | |
Posts: 4 Rating: (1) |
ok. i downlaod for DriveMonitor V5.5SP2 zip folder,11769381_drivemonitor_v5_5_sp2.zip (466,2 MB) afterwards not clear. |
2/16/2018 7:59 AM | |
Posts: 40 Rating: (0) |
|
2/27/2018 10:14 AM | |
Posts: 1 Rating: (0) |
Last day I tried to install DRIVEMONITOR on windows 10 but it can't install. It shows storage issues than, i contact How to solve Windows 10 storage problem they provide me the solution it helps me a lot. They told me to clean up the disk to have the free space. One can also delete the temporary files and recycle bin folders. if you are facing such issues follow this solution. |
Follow us on