2/5/2016 3:02 PM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33164 Rating: (4097) |
In the appendix an example. The address of the network input and the network output necessarily be the same. AttachmentV_pulse.zip (1052 Downloads) |
This contribution was helpful to3 thankful Users |
2/7/2016 2:09 PM | |
Posts: 2 Rating: (0) |
It works, thank you very much |
This contribution was helpful to2 thankful Users |
2/7/2016 3:03 PM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33164 Rating: (4097) |
Hello gregorIII, you're welcome. |
3/14/2016 7:21 AM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33164 Rating: (4097) |
Hello Zymo, the "forming" of a static network input to a pulse does not work in the simulation, but only in the real logo. In attachment a screen video. There you can see the program in online mode and place of the app I use the web server. As you can see, you can also switch multiple network inputs or pushbuttons connected to digital inputs in parallel. but it is always important, which is used during network entry, a network output with the same address. AttachmentTest.zip (609 Downloads) |
This contribution was helpful to1 thankful Users |
3/14/2016 12:50 PM | |
Posts: 6 Rating: (0) |
Dear Ixo65,
I will give this a try! Z |
This contribution was helpful to1 thankful Users |
Follow us on