1/2/2014 10:07 AM | |
Joined: 4/22/2010 Last visit: 10/17/2024 Posts: 5697 Rating: (715) |
Hello, Maybe attached document can be of any help. Regards, Marcjan AttachmentPDF_MM440_Masterdrive_braking_unit_en_V4_1.pdf (648 Downloads) |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
1/2/2014 10:49 AM | |
Joined: 10/11/2006 Last visit: 10/18/2024 Posts: 5925 Rating: (810)
|
Hello Piscean, the docu for the braking unit is found on the DriveMonitors DVD below options / components. There has been a modification with the braking units: The functionality is the same, the newer ones are now digitised and do have a open collector output instead a relais output, like the older ones have. The new braking unist are building smaller as well and thes don't have for the small sizes an internal Resistor anymore. The description "ba_bremsein_d_e.pdf" is for the older ones. The description "ba_bremsein_komp_5spr.pdf" is for the newer ones. An interesting link: http://support.automation.siemens.com/WW/view/en/11033894 |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on