5/16/2012 5:37 PM | |
Posts: 767 Rating:
|
Hello Genady, I do not recognize completely from picture of that specific part. Attached pdf may help as this may be the specific part, especially if there are three side by side on drive. You may contact below number to get direction to contact a Siemens repair center representative which could help further including repair itself. Contact Siemens at 1-800-241-4453 if you have other repair-related questions. AttachmentSpare Parts Pic.pdf (165 Downloads) |
5/16/2012 5:44 PM | |
Posts: 2 Rating:
|
how to get this pdf in full size? Thank you.
|
5/17/2012 1:14 AM | |
Joined: 6/4/2008 Last visit: 6/14/2024 Posts: 1484 Rating:
|
Hi Genady, I have included the parts list (in case you need some other parts) and a zoomed picture, but they are pretty low resolution to start with. I don't think the device is a transistor/mosfet, I believe it is a resistor, it is the same package size as the snubber resistors from the larger frame sizes (of which there are usually 6 of them), but in the case of smaller drives, I think it is the balancing resistor. This acts as a potential divider and creates a 0VDC point from which the power transistors can switch. Thats my guess anyway. Regards, Graeme
Attachment6se7024-7ed61.pdf (210 Downloads) |
This contribution was helpful to
1 thankful Users |
5/21/2012 10:54 PM | |
Joined: 6/4/2008 Last visit: 6/14/2024 Posts: 1484 Rating:
|
Genady, I just found this exact question and picture on aRussian website. Are you Onil?? Привет отSiemensфорум Regards, Graeme
|
Follow us on