5/17/2012 8:01 PM | |
Posts: 559 Rating:
|
Dear fhope, I don't know what you wan to say. But may the things described below may be helpful to you. If your CPU has programmed with some logic earlier & that program was saved in Flash card. Because we can download program into Flash during CPU stop mode only. If after that your programmer has changed some logic & he didn't downloaded that logic into flash card because of any problem say CPU stop mode was not possible. And now if your battery is also empty & Your CPU Power supply has been lost. So what happen, because of no battery backup the whole new backup from CPU will be lost. And Once you start the CPU again after giving Power it will take the backup from Flash card in which your old backup was available. Please check that may be reason in your case. |
5/21/2012 10:49 AM | |
Posts: 3 Rating:
|
This is the HW Config, its suppose to be Hot restart? Cold restart is not possible to select. |
5/21/2012 11:23 AM | |
Posts: 691 Rating:
|
Try Download User Program to Memory Card |
Follow us on