4/24/2018 8:29 PM | |
Joined: 9/26/2011 Last visit: 9/9/2022 Posts: 24 Rating: (0) |
Hi, I've change the CPU type to 412- 2 DP in HW configuration. after that CPU's "I ADDRESSES" in HW Configuration was differ than the old CPU. So i change all Device's Diagnostic Addresses according to the new CPU. the i Compile, Save and download to the target system. But CPU operating mode set to stop after run light blinks for few seconds. I've check CPU's Diagnostic Buffer but did not understand the Error. for reference see the Diagnostic buffer file. AttachmentDiagnose_New.txt (1074 Downloads) |
Follow us on