1/29/2009 7:37 AM | |
Posts: 20 Rating:
|
Thank you for this reply. How do you manipulate the header ? |
1/30/2009 9:15 PM | |
Posts: 2661 Rating:
|
Hi, Look at the attachment for example using CPU948. You need to be very proficient in STL to try this. I suggest you read thoroughly chapter 8 in the 948 manual from following link: S5-155U CPU 948 Programming Guide Unfortunately I cannot provide a cut-and-dried solution because: a) I haven't touched S5 for many years(>10) and b) I do not have S5 software and system to work on... But I remember implementing this in S5-150A/K/S/U & 110A/S. If I remember right, the way it works is, when you try to open a protected block it asks for a LIB= number and you have to enter this number right to see the code. Regards AttachmentCPU948_SoftwareProtection.pdf (436 Downloads) |
2/4/2009 10:09 PM | |
Posts: 2661 Rating:
|
Hi, Unfortunately the information about RS 101 to RS 127 is not provided in the system memory table as you can see from the attachment. Your best bet is to approach the Siemens Tech Support... Sorry couldn't be of more help... Good luck. AttachmentSystemArea_95U.pdf (545 Downloads) |
2/10/2009 6:35 PM | |
Posts: 2661 Rating:
|
Hi Late, I need to try this but I believe it'll work... Regards |
Follow us on