12/10/2007 3:05 PM | |
Posts: 2 Rating: (0) |
Purpose is for dosing predefined amount (by levelsensors)of chemicals to bath. Attachmenttestenkeldos.zip (656 Downloads) |
12/10/2007 4:26 PM | |
Posts: 661 Rating: (123) |
Hello jaws, please have a look at my file (see my part marked with "C1", "C2", "C3"). For each Cursor Key i´ve added some timers and counters to get the pulses. You have 5 seconds to count up the timers (off-delay), the they will start to pulse (edge triggered wiping relay). At the same time the counters will decrement. Unfortunately all 24 flags are used. To realize the 4th part "C4" you will have to free one flag (e.g. flag 5 is not necessary as far as i see). For a better understanding i´ve also attachedthe counter part without your program. I hope this is what you want to do. Regards Fux Attachmenttestenkeldos.zip (669 Downloads) |
12/10/2007 4:36 PM | |
Posts: 2 Rating: (0) |
Thanks, that's fast. I will try tomorrow morning if it works. With regards, Jaws |
12/10/2007 10:36 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580) |
Hello jaws, if the function from fux is right for your application, then look at my solution, it needs only 5 units instead of 6 and only 1 digital flags instead of 2! Now you must only use the counter values in your sheed.... If you not only want to tap for each input, you can add an impulsgeneratorbetween C2 and B009withpin INV inverted. Impulstime is in this case the waittime for the repeated autotap and Th+TL is the reparted time, but 1 unit more is needed! Best regards Betel AttachmentSchaltplan1.zip (679 Downloads) |
==> Meine TAG-Listen: "deut." |
|
Follow us on