Industry Online Support
Technical Forum
7/3/2013 12:24 PM | |
Posts: 1 Rating: (0) |
Hi everybody! Please help me to figure out this problem. My project in Braumat V6.0 SP2 including: 2 PC Servers (IOS01 and IOS02), 4 Clients (IOS11, IOS12, IOS21, IOS22), 2 PLC (PCU01 and PCU02). 2 PC Servers run redundancy. Server IOS01 controls PCU01, only reads PCU02 and has some recipes. Server IOS02 controls PCU02, only reads PCU01 and has also some recipes. 2 servers run redundancy as well in monitoring, control ICMs... but Recipe and Oder don't run redundancy. It means that if Recipe Server is actived in server IOS01, all of recipe and order in IOS01 can run as well; however all of recipes and orders in IOS02 can not run. In this case, I also try to start Order of IOS02 in IOS01, but the order can not run and status : released. My question is: How to configure to recipe redundancy? I want to start Order in 2 Server at the same time. I attached a file sys.ini of IOS02. Thank you for your supports
AttachmentSYS.zip (587 Downloads) |
Last edited by: Sandwich at: 7/3/2013 12:26 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on