7/20/2020 4:41 PM | |
Joined: 9/21/2011 Last visit: 10/24/2024 Posts: 3 Rating: (0) |
Hello, I'm testing Safety Evaluation function in TIA Selection Tool (a replacement for Safety Evaluation Tool). I created a simple configuration with an emergency stop pushbutton, safety PLC S7-1200 and third-party contactors to stop the motor. All subsystems (acquire, evaluate and react) have SIL CL 3 and very good PFHd, but the SRECS achieved SIL 1 only! SRECS PFHd achiever is 7.68E-09. SRECS SIL achieved should be SIL 3 in my opinion. Am I doing something wrong? AttachmentSafety Evaluation Report.Pdf (363 Downloads) |
Follow us on