Industry Online Support
Technical Forum
8/11/2023 7:13 PM | |
Joined: 10/15/2022 Last visit: 6/20/2024 Posts: 66 Rating:
|
Hi, LOGO! people. This program turns the outputs on or off with a delay. You can adjust delays separately. In the event of a power failure, the timers both delays resetted. True on-off delay timer differs from a standard on/off delay timer that when the timer is running (output high) and the input becomes 0 and 1 again (before the time is up) then the timer off-delay is not reset. Program "True on-off delay demo.zip" contains 5 files (program, UDF, schemes and description). Andrus AttachmentTrue on-off delay demo.zip (369 Downloads) |
Last edited by: Andrus_Saar at: 08/12/2023 06:35:00Last edited by: Andrus_Saar at: 08/12/2023 06:38:05 |
|
This contribution was helpful to
1 thankful Users |
Follow us on