5/24/2019 12:24 PM | |
Joined: 4/14/2010 Last visit: 5/14/2024 Posts: 525 Rating: (11) |
Greeting, Could you please suggest the upgradation of following YSKAWA servo system to SIEMENS drive technology. YASKAWA SERVOPACK Drive Model SGDH-02AE-S = 02nos. Input 1~ 220VAC 50Hz 3.4A Output 3~ 0-230VAC 0-300Hz 2.1A 0.2KW YASKAWA AC Servo Motor SGMAH-02AAF41 = 02nos. 200W 200V 2.1A r/min 3000 Nm 0.637 YASKAWA SERVOPACK Drive Model SGDH-15AE-S = 02nos. Input 1~ 220VAC 50Hz 19A Output 3~ 0-230VAC 0-300Hz 11.6A 1.5KW YASKAWA AC Servo Motor SGMGH-13ACA61 = 02nos.
1300W 200V 10.7A r/min 1500 Nm 8.34 Attachmentmotors & drives.zip (167 Downloads) |
MS |
|
5/24/2019 2:43 PM | |
Joined: 10/11/2006 Last visit: 6/5/2024 Posts: 5857 Rating: (793)
|
Hello, maybe V90 or S210 is an option. S210 https://support.industry.siemens.com/cs/ww/en/view/109754381 V90 https://support.industry.siemens.com/cs/ww/en/view/109758233 |
With best regards, |
|
6/25/2019 11:56 AM | |
Joined: 4/14/2010 Last visit: 5/14/2024 Posts: 525 Rating: (11) |
Thank You! Technology Team, What is your opinion and is it possible to make the compatibility with old motors and encoders,(attached) if we use the existing motor with new drives. YASKAWA AC Servo Motor SGMAH-02AAF41 200W 200V 2.1A r/min 3000 Nm 0.637 YASKAWA AC Servo Motor SGMGH-13ACA61 1300W 200V 10.7A r/min 1500 Nm 8.34
AttachmentMotors.zip (124 Downloads) |
Last edited by: MS1981 at: 06/25/2019 13:03:51MS |
|
6/25/2019 12:57 PM | |
Joined: 4/14/2010 Last visit: 5/14/2024 Posts: 525 Rating: (11) |
SINAMICS S210: Power Range S210 230 V 1 AC, 0.1 kW - 0.75 kW 400 V 3 AC, 0.4 kW - 7 kW (available soon) SIMOTICS S-1FK2: 0,05 kW - 0,75 kW 0,4 kW - 7 kW (available soon) Controllers SIMATIC S7-1500 T-CPU / SIMOTION Suitable application for Positioning of individual or multiple coordinated axes. SINAMICS V90 Power Range of 0.05 to 7.0 kW SIMOTICS S-1FL6 Servo Motors Controller SIMATIC S7-1200, SIMATIC S7-1500 inkl. T-CPU Suitable application for Positioning of individual or multiple coordinated axes. |
MS |
|
Follow us on