Industry Online Support
Technical Forum
11/10/2010 11:44 AM | |
Joined: 11/10/2010 Last visit: 6/5/2024 Posts: 165 Rating: (8) |
Hello, I'm doing tests on two CPU 313C-2DP, I have no ET200M redundant in stock, so I did the test with only two CPUs, the result in the status word redundancy in both CPUs is: 1 - For CPU A: 2 # 0010_0000_0000_0110 2 - For CPU B: 2 # 0010_0000_0000_1010 Which mean that both CPUs are spirit to operate in slave mode !!!!!? no master. Can you have an idea? I thought maybe I can not have a master in the absence of ET200M! Splitted from Redundancy. |
Last edited by: O_Moderator at: 11/11/2010 12:36 PMnew subject after splitting |
|
11/11/2010 12:37 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread redundancy with S7 313C-2DP. Best regards O_Moderator |
Follow us on