Industry Online Support
Technical Forum
8/20/2013 9:32 PM | |
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365) |
Hello, Why do we frequently miss links to samples as part of support.As previously discssed on " SIMATIC NET Quick Start Collection" issue HERE :
now I have problem finding a link that I was quoted as reference material for SIMATIC PID Self Tuner Package: PID Self Tuner: Example Adapted to Standard PID Control V5.1 My question is : if these changes and integration to new platforms are part of development, should not this switchover from old system to new platform make trouble for customers? My suggestion would be keep the old system working, customers have access to data available.Develop the new platform in parallel and switch to new system with re-direction of all old links to new pages.While encountering the page in attachment,Personally I should ask moderators and wait to get result.I am sure that will decrease the customer satisfaction of service provided here. Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 8/20/2013 9:34 PM// typo |
|
This contribution was helpful to5 thankful Users |
Follow us on