3/23/2016 6:00 AM | |
Joined: 7/4/2014 Last visit: 4/28/2024 Posts: 283 Rating: (0) |
Dear Sir
Thanks
Pl refer to attached S7zip from existing S5.Will it be possible for you to confirm if original .S5D got converted in to S7 completely or not ?
Before starting conversion, window shows
No Name Default New No
FB240 CODE:B4 " FC81 FB241 CODE:16 " FC82 FB242 MUL:16 " FC83 FB243 DIV:16 " FC84 FB250 RLG:AE FC0 FB251 RLG:AA FC1 OB1 OB1 OB31 OB31 PB1 FC2 PB2 FC3 PB3 FC4 PB4 FC5 PB5 FC6 PB6 FC7 PB7 FC8 PB12 FC9 PB13 FC10 DB1 DB1
I have clicked on Start then a the end of conversion 2 errors and 11 warning appeared
Warnings wrt FB240, FB242 - Preheader does not exisit, Invalid address. Errors wrt OB31
As FB240,FB22,OB31 do not exisit in New Number, do we need to correct these if yes then please let us know how to correct
Warm Regards Attachment483s7300.zip (203 Downloads) |
3/23/2016 6:10 AM | |
Joined: 7/4/2014 Last visit: 4/28/2024 Posts: 283 Rating: (0) |
Dear Sir Pl refer to attached zip folder consisting of S5 program which is running in the machine, along with list of old and new blocks before starting conversion , errors and warnings at the end of conversion. I have not done anything to correct Errors and warnings, as it is not clear on how to correct these errors or warnings In my previous post , I have also attached converted S7 project Kindly confirm if conversion is complete (as there were 2 erros and 11 warnings) or anything else we need to do to make the conversion complete and ready to Upload in S7300 CPU Regards Attachment50-0483.zip (208 Downloads) |
3/23/2016 11:14 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by Ertapu is split to a separate thread with the subject Convert program of s5 to s7 file, got No. of errors. Best regards |
Follow us on