3/11/2019 5:48 PM | |
Posts: 8 Rating: (0) |
HELLO PLZ HOW CAN I TRANSFER PROGRAM FROM WINCC TO TP 177B 6" color PN/DP WITH ETHERNET ? |
3/11/2019 6:35 PM | |
Joined: 3/28/2015 Last visit: 5/25/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following FAQs might help: 1-How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel? Download: 23800567_WinCC_flexible_Ethernet_Transfer_en.pdf 2-How do you use WinCC flexible to transfer a project to an operator panel via S7 Routing? |
Eng.Mohamed Ibrahim |
|
Follow us on