7/3/2014 5:49 PM | |
Posts: 69 Rating: (0) |
Hi I am using a (6es7 334-0ce01-0aa0) analog module and are trying to converte 0-20mA signals to 4-20mA any help will be extremely appreciated
|
7/4/2014 9:35 AM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hi! What do you mean for "convert 0..20 to 4..20 mA"? If you want to measure at 0..20 mA input and control 4..20 mA output, you will need another AO module or you can use third-party signal converter. Example of such converter can be foundhere(make sure to carefully read the manual before purchasing). If I misunderstood you, please specify your problem more detailed. BR, olloy |
7/4/2014 5:09 PM | |
Posts: 69 Rating: (0) |
Hi daniel So this means that it is not possible to scale it in any way ? am i tied to the 0-20ma on the inputs and outputs ?
|
7/4/2014 5:28 PM | |
Joined: 1/21/2013 Last visit: 10/8/2024 Posts: 4620 Rating: (708) |
Hello Mishal11, Havea look here, if you can help: How can you standardize and destandardize analog values with STEP 7 V5.5? |
Follow us on