8/26/2016 11:53 AM | |
Joined: 5/20/2015 Last visit: 6/13/2024 Posts: 216 Rating: (3) |
hi guys i have requirement of 100% redundant PLC system, in Which about 60 to 70 PID controls are required, Now i dont know that which PLC system has to be implements for this project ie s7- 300/400/1500. Also i have doubt that "IS THERE ANY MODEL OF S7-1500 WITH 100% REDUNDANCY?", if not then which PLC i need to use where total Power tags are under 400 numbers. thank you. Regards Gabbar.. ------------------------------------------------------------------------------------------ |
Last edited by: gabbar at: 8/26/2016 12:31:24 PMLast edited by: Min_Moderator at: 8/26/2016 2:11:18 PMNew subject after splitting Let's do it... |
|
This contribution was helpful to1 thankful Users |
8/26/2016 2:55 PM | |
Joined: 5/20/2015 Last visit: 6/13/2024 Posts: 216 Rating: (3) |
thank you guys, for yours valuable information. |
Let's do it... |
|
Follow us on