5/21/2014 9:56 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello JordiHelixFlay This is effectivaly One 2-Port Ethernet switch built into the CPU so it willhave only One MAC address and one IP Address. Normally any switch / router will have only one MAC address and one I.P. address. If you want two separate MAC Addresses / IP Address , you may consider adding a CP 343-1 Ethernet card to the CPU. Thatway you can have two separete Ethernet networks with different MAC Address andIP Addresses. Hope this helps Cheers Navnag |
Last edited by: Navnag at: 5/21/2014 9:57 AMThere is no such thing as the last bug in a program |
|
This contribution was helpful to3 thankful Users |
5/21/2014 11:29 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello JordiHelixFlay Have you already seen this Perhaps this might help: MAC adresses CPU317F-2PN/DP |
This contribution was helpful to1 thankful Users |
5/27/2014 7:34 AM |
|
Joined: 4/17/2012 Last visit: 3/30/2024 Posts: 474 Rating: (10) |
Hi, it is like a parallel port so it won't have one more ip address |
Follow us on