9/10/2018 2:45 AM | |
Posts: 9 Rating: (0) |
Hello Sir Thank you for repling. Please see the attached file for full view. Our system is using CPU948R for redundant which is using IM308-C to connect to field device. Thank you for helping. Attachmentfault.pdf (362 Downloads) |
9/12/2018 9:39 AM | |
Posts: 9 Rating: (0) |
Hello Sirs There is nothing on AP, but the errors comming and going to OM every 30 minutes(please see the attached file). I've checked on SIM , there is nothing, that is switched I/O with IM308-C on every CPU and 2 IM153-2 modules on every station. There is error in the log relative to PB108 and PB119 but I can nor see any PBs like that in the program. There is not process running every 30 minutes in the program and I do not know how much time cycle interrupt in the process, sorry about this. And one more question, there are 5 DIs module , so how to know the address of every DI module? Thank you very much Attachmentproblem-12-09-18.pdf (340 Downloads) |
9/15/2018 3:14 AM | |
Posts: 9 Rating: (0) |
Hello Sir. That's correct, It' s TXP .and 21CJF01.DA19 is CPU-A . I've changed everything to the good one included: Subrack, CPUA/B, IM314/324R; IM308-C but it's still problem. Yes, there is a DS670 here(please see the attached picture) Yesterday, I tried to change Digital input module 4 of 5 stations but the problem was still there. Today I will try to change the last station. Thank you very much. Attachmentds670.docx (300 Downloads) |
9/18/2018 2:55 AM | |
Posts: 9 Rating: (0) |
Hello, Please see the attached file. By the way, the system is connected to the field device using profibus-DP through IM308-C(6ES5308-3UC21); the system is connected to S5-95F through CP530(6ES5530-3LA12). Thank you. AttachmentRack view.pdf (331 Downloads) |
Follow us on