1/18/2020 12:51 PM | |
Posts: 1 Rating: (0) |
Start CPU from scratch with an Eprom or an EEprom. Yes you can store the Eprom, make sure the little window on the Eprom itself is covered and keep away from direct light, better get an EEprom or spare Eprom.
I have followed your instructions like above but it works as long as there is a Eprom in the CPU.. I used an CPU 943 from the 115U series. When I remove the module it doesn't work, so the programm is not in the CPU memory. How can i get the programm in to the CPU memory again? ------------------------------------------------------------------------------------------ |
Last edited by: Marc@S5 at: 01/18/2020 13:44:39Last edited by: Jen_Moderator at: 01/20/2020 06:10:55New subject after splitting |
|
Follow us on