1/24/2023 7:03 PM | |
Joined: 12/18/2014 Last visit: 6/10/2024 Posts: 33176 Rating: (4101) |
I have installed STEP7 V5.6 SP2 HF7 und and the HSP0242 is installed. |
2/21/2024 1:49 PM | |
Joined: 10/11/2011 Last visit: 5/16/2024 Posts: 9 Rating: (2) |
Altough this thread is a bit old it should be never too late to publish a fix. I got the certificates updated on the exact same step 7 and windows version as stated here. Then i got the newest HSP file updated. In the appendix I included a small manual and a updated certificate file as of 21-2-2024. The update file that makes you able to update the certificates manually in windows 7 are provided in the manual. Hope it helps someone. AttachmentHW update problem step 7.zip (228 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on