1/27/2022 5:24 AM | |
Joined: 10/18/2014 Last visit: 4/11/2024 Posts: 10 Rating: (0) |
IS PCS7 V9.0 SP2 COMPATIBLE WITH WINDOWS 10 ENTERPRISE LTSC OR NOT? I HAVE INSTALLED CLIENT AND DOWNLOAD FROM ES BUT WINCC NOT RUN. I GET THIS INFORMATION. "THE PROJECT COULD NOT BE OPENED.ERROR:CANNOT OPEN OR START WINCC PROJECT,AS PROJECT MANAGER CANNOT START BASIC APPLICATION XREF" PLEASE GUIDE ME. THANK YOU ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/27/2022 11:42:26New subject after splitting |
|
1/27/2022 7:26 AM | |
Joined: 9/3/2008 Last visit: 5/3/2024 Posts: 921 Rating: (158) |
Hello, Did you look in the readme for the requirements: https://support.industry.siemens.com/cs/ww/en/view/109760505/130814951435 You can also look in the Compatibility Tool: https://support.industry.siemens.com/cs/ww/en/view/64847781 Regards Michael |
Last edited by: Michael K at: 01/27/2022 07:28:04Michael |
|
1/27/2022 11:39 AM | |
Joined: 2/17/2020 Last visit: 5/3/2024 Posts: 995 Rating: (170) |
Hi Farid Kahn, It seems that it only supports Windows 10 Enterprise LTSB or LTSC 2015 (64-Bit). AttachmentPCS-7_V9.0_compatibility-list_en_2022-01-20.zip (265 Downloads) |
A rating will be well appreciated. |
|
Follow us on